Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Tiva C Series TM4C123x Family of MCUs Slide 14

The ADC module can also be used to generate interrupts when a sample sequencer completes sampling a signal, when hardware sample averaging circuit completes sample averaging, or when a particular voltage is seen on an input of digital comparator, based on mode of operation. The register configurations of the sample sequencers and digital comparators dictate which events generate raw interrupts, but do not have control over whether the interrupt is actually sent to the interrupt controller.

PTM Published on: 2013-09-10